EEO#.PULSEWIDTH

Description

The pulse width of the pulses from the CW/CCW and step/dir modes,EEO#.MODE 1 or 2. In these modes this parameter also controls the width of the Z pulse. This parameter has no effect in the A quad B mode.


  • If the pulse width is too long it will effect the maximum speed of the output as the pulses will start to overlap. This formula is expressed as:
    MaxVelocity (rev/sec) <= 1/(Lines * PulseWidth_in_secs).

Examples

Code

This will set the pulse width to 8.16 us.

-->EEO1.PULSEWIDTH 8.16

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units us
Range 0.08 to 2621.40
Default Value 4.08
Data Type Float
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen